Hi Dear,
Our customer uses DRV2700, the load is piezoelectric ceramics, and the hardware is made according to the reference design of DRV2700EVM-HV500.
The output scheme is selected as shown in the following figure. After testing, the ripple at the output end is too large, even nearly 20V, may I ask if there is any way to reduce the ripple?