This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8316A: not detect Speed Out from DACOUT

Part Number: MCT8316A

Hi,

I am using MCT8316AEVM.

To measureing Speed Out, set [DAC_SOX_CONFIG] to "DACOUT2" and set [DACOUT2_VAR_ADDR] to "Speed Out(0x5AA)" . 

But "DACOUT2/SOX" outputs no signal.

After I tried to change  [DACOUT2_VAR_ADDR] to "Input Duty Cycle(0x40C)" , I confirmed "DACOUT2/SOX" outputs signal.

But, when  [DACOUT2_VAR_ADDR]  is set to "Current Duty Cycle" , "3ph Duty cycle","Closed loop speed Ref", "AVS Ramp Down Duty","Speed Equiv. Duty",

there was no signal like "Speed Out"

Do I need to configure something else to cofirm signal?

Best regards

Yuki