This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8316: DRV8316TRGFR

Part Number: DRV8316


We would like to use the DRV8316CTRGFR but there appears to be no stock. Is this a valid part? 

Also is there a version of the DRV8316xEVM with the hardware interface variant (DRV8316T)? If so how would I order one. 

  • Hi Roy,

    Thank you for posting to the Motor Driver's forum!

    The DRV8316CTRGFR is a valid part, however, due to high demand in the market, the current lead time is 6+ weeks. Please plan for such lead times as you submit orders.

    The DRV8316xEVM comes populated with the SPI variant, though it is compatible with the DRV8316T (H/W variant). Please see section 4.1.1 DRV8316T Compatibility for more information. You would need to depopulate the SPI variant and populate it with the H/W variant.

    Best,

    ~Alicia