This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353: charge pump sometimes stops functioning

Part Number: DRV8353


Dear forum members

We have occasional problems with the charge pump.

when the DRV8353 works at VM=24V the device works without any problem but if the VM=52V the charge pump sometimes stops functioning, fault is active and the VCP voltage is VM-0.3V
In such a situation, the current consumption of the DRV8353 is about ~70mA and we have to replace the DRV8353

Best Regards
Shaya