Hello all,
I've got a custom application and made a custom GUI to read and write the registers of the MCT. However when writing 0x80000000 to register ALGO_CTRL1 as written in 8.6.1.1 EEPROM Write in the datasheet, it does not actually write it. Ive read the other forum posts, and made sure the state machine is in state 6 (MOTOR_IDLE) while writing the value.

The state can be seen in the bottom left, "STATE: 6".
When enabling the toggle button, it writes the value to the register.
However, when after some time enabling the EEPROM_READ bit, all values change back to the original default values.
Could it be the value of the EEPROM_WRITE_ACCESS_KEY shouldn't be 0?
Thanks!
Marcel