Other Parts Discussed in Thread: DRV8714-Q1
Hello Team,
customer has a question regarding both DRV8718S and DRV8245 ICs:
Will these devices lose control of the Gate/input signal when exposed to a negative gate to source bias? This can generally occur if the device has an open circuit (gate/input is near zero volts (commanded OFF) and the source is pulled high via a current source on the output used for open circuit detection, or if the source/output is shorted to battery). Can ion-migration occur resulting in a Vt shift, which may allow the device to be partially ON when the gate/input is OFF?
Many Thanks
Josef