Hi,
Can I use MCF8315A or MCF83EVM to control 24V, 3 Watt, AC synchronous motor? If you need motor details, please PM me.
Or, if you have better suggestions for AC synchronous motor controller, please let me know as well.
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can I use MCF8315A or MCF83EVM to control 24V, 3 Watt, AC synchronous motor? If you need motor details, please PM me.
Or, if you have better suggestions for AC synchronous motor controller, please let me know as well.
Thanks,
Does your motor have permanent magnets on the rotor? if yes, then you can use MCF8315A to drive your motor.
Hi,
MCF8315 is 3 phase. The Motor that I'm trying to control is single phase. Do you have PMSM controller with single phase? Thanks
Hello,
By 4W1-2 Phase Excitation, I think this is the same as our 1/16 microstepping mode. Many of our stepper motor drivers support microstepping. See the following link, any driver with 16 or 256 microstepping levels will be able to do 1/16 microstepping: https://www.ti.com/motor-drivers/stepper-driver/products.html#2894=16%3B32%3B256&
24V 3W is 8 amps, our only stepper motor driver with microstepping that could drive this load is the DRV8462.
You might also find this reference design guide useful: 48-V, 10-A, High-Frequency PWM, 3-Phase GaN Inverter Reference Design for High-Speed Motor Drives (Rev. B)
Regards,
Jacob