Other Parts Discussed in Thread: DRV2511Q1EVM, , MSP-EXP430G2ET
Hi Sirs
We would like to develop MCU MSP430 to driver DRV2511Q1 for haptic test
Inquire
1. Sample code
2. Register setting
Sincerely
Jax
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sirs
We would like to develop MCU MSP430 to driver DRV2511Q1 for haptic test
Inquire
1. Sample code
2. Register setting
Sincerely
Jax
Hi Jax,
You can find the firmware from the DRV2511Q1EVM here as a resource: https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/688133/ccs-drv2511q1evm-drv2511q1evm-firmware-code
This EVM already uses a MSP430 to drive the DRV2511Q1. The DRV2511Q1 does not have register settings. It is a hardware controlled device.
Best regards,
Jeff McPherson
1. How to import to Haptic Control console?
What do you want to import? Please clarify
2. Does it have any guideline to apply this FW?
The firmware can be downloaded to the EVM easily through Haptic Control Console. Editing the firmware is available for advanced and experienced users only so there is no documentation on that.
Best regards,
Jeff McPherson
Hi Jax,
Be aware that HCC is only compatible with the EVM. If you are using the EVM, HCC has a firmware updater built in that will allow you to update the EVM to the latest firmware. You can find the updater by clicking "Help" -> "Firmware Update." The firmware update file will be available inside HCC. Be aware that HCC is not able to open and edit firmware. That can only be done in Code Composer Studio.
Best regards,
Jeff McPherson
Hi Sirs
Goal: Develop solenoid driver with TI MCU with Code composer studio
Prepared: TI Launch Pad kit(MSP-EXP430G2ET), DRV2511-Q1 EVM kit, USB2UANY
Inquire:
1. Do we need other device or accessories
2. How to set up DRV2511-Q1 environment with Code Composer studio and above HW device?
3.. Does CCS has sample code?
Sincerely
Jax
Hi Jax,
You shouldn't need any other accessories or devices. To set up the environment please refer to the firmware shared earlier. That will be your example code.
I am only an expert in the DRV2511-Q1. For more detailed support on CCS and using the MSP, please make a ticket with the processors team.
Best regards,
Jeff McPherson