Hello
I have an application where I'd like to fix the LRM frequency at ~170Hz - no auto resonance desired.
Is this achievable by doing the following?
- Set LRA_OPEN_LOOP bit to 1 in register 0x1D
- Set N_ERM_LRA bit to 1 in register 0x1A
- Set DRIVE_TIME[4:0] to 24 in register 0x1B
Thanks!