This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8329EVM: Reverse rotation is not working on forward reverse mode. How should I set appropriate values on registers?

Part Number: MCT8329EVM


I am trying to turn BLDC with MCT8329EVM. I am trying to give the RPM command by PWM Duty: Stop = 1.5ms, Forward Max = 1.9ms, Reverse Min = 1.1ms.
Please tell me about the following

1) I am trying to give instructions for forward and reverse rotation using the attached map and register settings.

The reverse side can be controlled at variable speeds appropriately. However the forward side does not rotate at all. How can I get the forward side to rotate as well?

(2) As mentioned above, the original PWM Duty range is Stop = 1.5ms, Forward Max = 1.9ms, and Reverse Min = 1.1ms.

To achieve this operation, I think Forward and Reverse must be reversed. Could you please tell me how to reverse the direction of rotation?

20230724_Motor_Controller.pdf