This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8343-Q1: DRV8343-Q1 motor driver in rhe 1 x PWM—Hall Effect Sensor mode

Part Number: DRV8343-Q1


Dear User,

I use the DRV8343-Q1 motor driver in rhe 1 x PWM—Hall Effect Sensor mode.

What are the effects of the PWM fundamental frequency INHA, if I change this from 1kHz to 20kHz?

The motor speed is specified independently of the load via the pulse width of the basic frequency?

Thank you for an answer.