This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN1B044PWPR: internal equivalent circuit diagram of terminal block

Hi,

Do you have an internal equivalent circuit diagram for the terminals?

Especially for the following signal input terminals:
・CLKIN/ACCn/PWMIN terminal (11pin)
・DECn /ENBLn terminal (12pin)

I want to know the internal resistance and configuration of the terminal part for voltage level matching of the terminal when connected to an external circuit.

Regards,