I am trying to use DRV2700EVM to drive a piezo actuator (P-602.3SL from PI) with a 3Hz sine wave (Output voltage -20V to 100V) . During operation I can observe drops in VBST probably because boost goes into over current mode .
The actuator is 3.1uF rated . I tried driving a 3.3uF capacitor with the same waveform and there I don't observe any problem.
Is there any issue driving an actuator with DRV2700EVM ?