Other Parts Discussed in Thread: INA236
hello.
I used a translator.
I am driving a BLDC motor with the DRV8306 motor driver.
I am reading data with ADC by connecting a differential amplifier to both ends of Rsense.
I found something strange while implementing current control with ADC data.
- When there is no load on the motor.
Power supply current value: 200mA
ADC value: 2000 - When there is a load on the motor.
Power supply current value: 300mA
ADC value: 2000
If the ADC value read from Rsense is the same, the current value of the power supply should be the same, but it is not.
I wonder why the current value of the power supply and the ADC value are different.
Best Regards
On