This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BLDC motor controller design suggestions

Other Parts Discussed in Thread: MCT8329A, DRV8306

Hello,

Our client has hired us to develop a BLDC motor controller for a battery operated application. We are looking for assistance in choosing optimal components for this design and possible existing reference designs to speed up the design phase.

Description of the application:

We are powering a 1.5kW BLDC motor with 18 Vdc rated voltage. If possible, we are looking for a controller which is capable of driving the motor on its own, meaning that the only input it requires is the speed / direction command (control algorithm implemented by the controller IC).

A housekeeping MCU is planned which will overview the user interface and give the speed commands to the motor.

Please let us know the suggested components which are applicable to our application.
Also, please let me know which additional information you require.

Thank you and best regards,

Samo Smodiš