Hello,
My customer is testing the DRV8870 operation on their custom board.
They designed as below.
- Sense Resistor = 0.1R, Vref = 3.3V, Current limit setting = 3.3A
It is confirmed that the 3.3A limit is applied to the motor outputs OUT1 and OUT2, and when the current of the motor input VM is measured, it is as follows.
There may be a Toff time in us units after the current limit, but if you look at the graph above, the current turns ON/OFF repeatedly every 200 mS.
(The 200ms cycle is not fixed, but slightly variable)
The actual motor is also turned on and off.
Is this symptom caused by lack of torque in the motor? Or is the DRV8870 limited as above?
Thank you.
JH