We're considering driving an inertial load using a BLDC motor driven by this part @66V.
Is it possible to implement regen braking even in the 1x PWM mode? The datasheet says that The INLC input brakes the motor by turning off all high-side MOSFETs and turning on all low-side MOSFETs when it is pulled low.
- Can the braking current be controlled using the bidirectional current sense amps? Will the DRV automatically enable cycle-by-cycle limits on the current similar to the forward mode? In such a scenario - during the cycle off time will the motor current feed back into the bus via the body diodes resulting in regen braking?
- If the above is not implemented, can a external PWM given to INLC implement regen braking?