This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8316Z: MCT8316Z

Part Number: MCT8316Z


I am doing some experiments with MCT8316ZEVM and have a question about a strange behaviour that i detected. There is a delay of about 1s until the motor reacts when the duty cycle of the PWM is changed from 0 to a certain value. The behavior only occurs when the duty cycle is changed from 0%. A change from e.g. 10% to 40% is accepted immediately.
What is the reason for this behavior and what can be done about it?