We prefer to use through hole package to the standard HTSSOP package, is there one available?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We prefer to use through hole package to the standard HTSSOP package, is there one available?
Hi Mohamed,
Unfortunately, we do not have through hole package for DRV10983.
Regards,
Vishnu
We need to manufacture our driver PCBs in-house. Our capabilities can support traditional but not HDI PCBs. Do you have any suggestion?
Like for example, is there any mounting kit that can do the adaptation?
We do not recommend mounting kit because we recommend the IC thermal pad to be in contact with the PCB for thermal heat dissipation. Unfortunately, I do not have any other suggestions.
So to use the PCB as the heat sink, is there a custom PCB design recommendation, I mean area, shape ....
Below are the two reference PCB designs we have for DRV10983. PCB files can be downloaded from the "Design files" section.
https://www.ti.com/tool/DRV10983EVM
https://www.ti.com/tool/DRV10983EVM-TB
Regards,
Vishnu
I checked both designs and need to confirm a point: DRV10983 is using the GND plane to dissipate heat. Practically, I can implement the whole design in one PCB layer. However, from heat sinking point of view, do we need both sides GND planes to dissipate the heat? or one side is enough?
Board size is 50 x 60 mm
We do not need both the side of the PCB to dissipate heat but if the device draws large currents or the PCB size is too small, we might see significant rise in temperature of the IC which can trigger Over temperature shutdown fault.