This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8262: Looking for integrated 24V automotive H-Bridge Driver with high output current

Part Number: DRV8262
Other Parts Discussed in Thread: DRV8873-Q1

We are looking for an integrated automotive grade H-Bridge driver for a 24V automotive design. Below are the key requirements of the H-Bridge driver:

Normal working voltage: 32V+

Supply voltage rating: 40V+, ideally 60V+

Number of bridges: 1+

Max output current: 6.7A+ DC, 2.5A+ rms

Max PWM frequency: 40KHz+

Max junction temperature: 125C+

DRV8262 fully meet the above requirements, but is not automotive qualified. Other automotive H-Bridge driver like DRV8873SPWPRQ1 (4A current rating) and DRV8243SQRXYRQ1 (max 25KHz PWM) don't fully meet the requirements.

Does TI plan to have DRV8262 automotive qualified soon with some degradations? Or there are other integrated H-Bridge drivers in TI's automotive road map that will meet the above requirements?

Thanks,

Charley