Hello,
We are using a DRV8353H to design a BLDC motor driver and have a few questions regarding the power supply recommendations
The external supply voltage range is 18-75V and we are using the dual power supply configuration with Vdrain connected to the external power supply and Vm connected to a 12-24V to reduce the internal power dissipation.
2*560 uF , 100V electrolytic capacitor and one 100uf , 35V ( rated for Vm) - would this meet the requirements for local bulk capacitance ? We are targeting output current of 15 A and instantaneous peak of 30A.
thanks
Najma