This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301: PWM issue

Part Number: DRV8301


Hi Team,

When using the DRV8301 to control a motor, the input upper PWM and the output PWM differ, causing problems with motor control. 

Could you help check this case? Thanks.

Best Regards,

Cherry

  • Hi Cherry, 

    Thank you for your question! 

    Can you clarify which phases/pins this issue is appearing on, and which are being shown in the waveform?

    And can you also provide the schematic and commutation method being used?

    Thank You and Best Regards,

    -Joshua

  • Hi Cherry, 

    It has been a little while without response and I will be closing this thread now. 

    If you have any additional comments, please respond or create another thread if there are further questions on the matter---always happy to help!

    Best Regards,

    -Joshua