This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2605LEVM-MD: DRV2605L Driver IC working with DMEGC DM-LM0710-8 LRA

Part Number: DRV2605LEVM-MD
Other Parts Discussed in Thread: DRV2605L

Hi,

I am working on an LRA "DMEGC DM-LM0710-8" using the board DRV2605LEVM-MD.

And comparing the result with another driver IC development Borad: Renesas / Dialog DA728x-EVAL-KIT.

We found that at the same Vrms output level:

- with Closed Loop function ON, the TI Driver runs at 231Hz, and produce a vibration force 2.6Grms

- with Auto tracking function ON, the Renesas / Dialog Driver runs at 246Hz, and produce a vibration force 8.7Grms

Looks like the TI Driver is not very good at finding the best resonance frequency for some LRA models.

Do you have any comment on this? Or do you have an upgraded driver IC model that can work better?