Hi Team,
If the customer would like to support a single BLDC, should they drive the DRV8962 inputs (IN1..3 and EN 1..3) in the right timing to create the rotation? Thanks.
Best Regards,
Cherry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
If the customer would like to support a single BLDC, should they drive the DRV8962 inputs (IN1..3 and EN 1..3) in the right timing to create the rotation? Thanks.
Best Regards,
Cherry
Hello Cherry,
Is there a reason the customer wants to use the DRV8962 instead of a dedicated BLDC driver. Can you give me the voltage, load current requirements and if you want an integrated FET and/or control solution, so we can recommend a BLDC driver if you want. You could use this driver, but you have to provide the right INx and ENx signals with an external microcontroller of some sort with the right sequence and timing between the signals.
Best,
Keerthi