Part Number: DRV8106-Q1
I'm evalutation DRV8106 Q1,
I manage to configure and start the HBridge, I've a 50% PWM @ 2 KHz on IN1.
I've command signal on GH1, and high side MOS is driven accordingly
No fault repoorted
CSA configured and current reading is plausible with ma load.
Issue: Low side MOS is not driven, GL1 remain to 0V
Question : Is there any register setting that may prevent GL1 and low side MOS to be driven ? ( if not, my EMV is likely broken)