Hello,
We are using a DRV8434SRGER under the following conditions, but it goes into thermal shutdown (OTSD).
The symptoms are the same for both the board we developed and the DRV8434SEVM board.
Could you please tell us the probable cause of this problem?
VM voltage: 24V
Vref voltage: 2.26V (@Vcc=3.3V)
Setting torque: 100%
Ambient temperature Ta: 25°C
Motor inductor: 6mH
Motor resistance: 1.7Ω
Best regards,
Naoki Takano