Hi Team,
The customer would like to make sure if DRV8323 still can be used if the voltage input pins do not match the bus voltage of the 3-phase inverter bridge? Thanks.
Best Regards,
Cherry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
The customer would like to make sure if DRV8323 still can be used if the voltage input pins do not match the bus voltage of the 3-phase inverter bridge? Thanks.
Best Regards,
Cherry
Hi Cherry,
The DRV8323 is not recommended to be used that way since it has a single-supply voltage architecture and not split-supply, like DRV835x family. VM being too different from VDRAIN may also result in VGS monitoring faults.
Hope this information is helpful.
Best Regards,
-Joshua