Other Parts Discussed in Thread: DRV8231A, DRV8231
Hi team,
There is a DRV8870 failure case need your comments. Customer find that there are two pcs DRV8870 broken down, and both are VM pin burned out.
Customer application: the VM voltage no higher than 17V, and the current not higher than 1.2A, both are far away the threshold and many buffer.
1. Could you help to provide your comments for the root cause of this case?
2. We find there is a similar case VM broken case in e2e forums, the link is https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1214985/drv8870-the-vm-power-pin-is-burned-out?tisearch=e2e-sitesearch&keymatch=DRV8870# . Do you think it is a comment problem in application?
3. Please help to provide comments about how to avoid this type failures?
Thank you.