This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8718-Q1: CSA output current capability

Part Number: DRV8718-Q1


Hi team,

What is the output capability of internal CSA?

From datasheet, I see max current is within 0 and 5mA. however, if calculating the current based on the output slew rate, it should be 150uA(60pF x 2.5V/us). which makes me confused, Could you help to check?

B&R

Lijia