This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8245-Q1: Current Scaling Factor tolerance AI_ERR

Part Number: DRV8245-Q1

We are using DRV8245SQRXZRQ1 in our design.

The current scaling factor AIPROPI value given for this part number is 6400.

But the tolerance value AI_ERR, is given only for the output current range of 0.2A < Iout < 10.9A, 

Our current in the design is maximum is 16.5A.

Kindly tell what is the tolerance we should use as the datasheet only provides upto 10.9A of Iout.