This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2700: Doubts whith the inputs conections

Part Number: DRV2700


Hello. ive been trying to understand how ca i use de inputs for this device. I guess that a can put a analog input at +IN pin and put the -In pin to gnd or a 0.1uf capacitor. Its is possible?

  • Hello,

    Thanks for reaching out. It depends on how you would like to set up the device. Section 8.1 Application Information in the DRV2700 data sheet has various diagrams for different applications. For it example, it has AC-Coupled DAC Input Application, Filtered AC Coupled Single-Ended PWM Input Application, DC-Coupled DAC Input Application, and DC-Coupled Reference Input Application. It sounds like you are wanting to do a single ended input. You can connect IN- with a cap to ground and then an AC coupled signal to IN+. 

    Regards,
    Sydney Northcutt