This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353: DRV8353- same gate drive current strength, but MOS-GS rise waveform is different

Part Number: DRV8353

Hi,Ti member

when  using DRV8353 to drive MOS ,found the rise time of high side MOS is different from the  low side MOS , 

  I had set the same IDRIVEP and IDRIVEN of High side MOS and Low side MOS ;

---Low side MOS-VGS waveform:

--High side MOS VGS waveform

as you can see , VGS voltage rises  from zero to Miller platform voltage,which is different

pls help me

in detail ,pls check the attachment

GS-waveform.ppt