Hi,
I am using the DRV2605L to design a prototype for a haptics based product. I am having issues getting the autocalibration to complete successfully. I am using an LRA in closed loop mode. The LRA has the following parameters:
- RMS Voltage: 2.83Vrms
- Resonant Frequency: 160Hz
I am using the following register settings:
- Feedback Register (0x1A): 0xB6
- Rated Voltage (0x16): 0x78
- Overdrive (0x17): 0xBD
- Control1 (0x1B): 0x1B
- Control2 (0x1C): 0x75
- Control3 (0x1D): 0x8C
- Control4 (0x1E): 0x40
I am using the Seeed Studio haptic motor v0.9 board connected to my haptic motor. Any suggestions on what I can try?
Thanks
Aaron