This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8143H-Q1EVM: D2 LED of DRV8143H-Q1EVM keeps blinking

Part Number: DRV8143H-Q1EVM

Hi~

When the DRV8143H-Q1EVM is connected to power, the D2 LED continues to blink. 

The jumper settings are as shown below. 

When the nFault jumper (J4, 9-10) is opened, the D2 LED turns off. 

I understand that nFault operates in Active Low when there is a problem with the DRV8143H-Q1. 

Even though the power supply and load connection are performed properly, the D2 LED blinks. 

What settings are causing the D2 LED to keep blinking?