Hi, all
I try to control the step motor using drv8818.
Question 1.
- When I put pulse on the STEP input pin, do I have to give it at 5V?
- It is currently connected to ST company's MCU pin, and the corresponding MCU VCC is 3.3V.
Question 2.
- Are the output waveforms of the AOUT1, AOUT2, BOUT1, and BOUT2 pins normal?

Yellow = AOUT1, Blue = AOUT2, Red = BOUT1, Green = BOUT2
the motor does not rotate and only vibrates.
I ask for help. Let me know if you need any additional information