Hello, I'm using the DRV2700 chip and designed a boost power supply PCB to elevate the voltage to 500V based on the boost circuit in the chip manual. After soldering, I found that without inputting a signal, the output voltage is only a few volts. However, it is increasing very, very slowly, and it is far from reaching the desired 500V. Could you please tell me if there is an issue with my circuit?