Part Number: DRV8245-Q1
While testing the ITRIP condition in DRV8245, independent mode.
Here, we have used 0.9ohm load resistor,16V with 100% duty cycle.
The output current waveform should TRIP at 12.6A( IPROPI resistance=1Kohm and ITRIP resistance=22.1Kohm) , means output current max should be 12.6A , but here it is reaching to 17A((load current at 16V,0.9ohm)) which is above the ITRIP current.
Waveforms are attached for your reference.
Is our understanding on ITRIP is correct?