This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8706-Q1: how to understand VGS_HS_DIS bit

Part Number: DRV8706-Q1


hi experts

how to understand the function of "VGS_HS_DIS" and the meaning of "handshake"? 

  • Hello,

    If this feature is ENABLED, then the device will measure the VGS on the gates of the external FETs and use this information to switch one FET "off" before switching the other FET "on".  This monitor works on both high-side and low-side FETs to avoid a shoot thru condition when both FETs are on at the same time.  The "handshake" ensures that one FET is off before enabling the other FET on.  

    It is a smart gate drive feature.  If you disable it, the device will act like a standard gate driver and obey the deadtime numbers without using the VGS monitors. 

    Regards,

    Ryan