This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV3256-Q1: Phase Comparator : Output on PHCx pins

Part Number: DRV3256-Q1


Hello Team,

I have some doubts related to the Phase comparator unit in DRV3256-Q1

Q1 --  As per the PHC_CTRL Register Field Descriptions,

When the PHC_TH is set to 1b0 = 75% for rising and 25% for falling , does this mean that the mis-compare will be reflected on PHC pin only when transition is happening (either falling edge or rising edge); or will it be also reflected when the SHx is at some fixed voltage level (for e.g. say 15% of DHCP).

Q2 -- Would be useful if you help me with the response of the PHCx pins as per below table

PHC_TH Voltage at SHx PHCx PIN STATE 
1b0= 75% for rising and 25% for falling Above 75% of DHCP  
Below 25% of DHCP  
Between above range  
1b1 = 50%  Above 50% of DHCP  
Below 50% of DHCP  

Thank you.