This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV120: Output (hold) current not achieved

Part Number: DRV120


Greetings. I am using the 8-pin DRV120, 24V source, 83ohm solenoid. With the 8 pin package, I cannot externally set the hold current - it should default to 50mA. However when the DRV120 is enabled, I'm only seeing ~10mA delivered (based on a bench supply readout). See below for the schematic, "VENT_OUT" goes to one side of the solenoid, the other side ties to the 24V supply. Insight appreciated, thanks!