Other Parts Discussed in Thread: DRV8824
The motor driver chip DRV8824 is set to 1/2 phase, and the software input STEP is fixed to 12PPS. However, the number of steps is inconsistent at the output of DRV 8824 (The actual number of steps tested on the motor side is greater than 12 steps). Please help with analysis and support, thank you!
This is the circuit schematic diagram:

This is the stepper motor drawing:

This is the waveform of STEP pin:

This is the waveform of Out,yellow is the waveform of the voltage probe, red is the waveform of the current probe.: