Hi team,
My customer set PVDD = 13.5V DVDD = 5V nSLEEP = 0V and test Iq. They tested 16mA on PVDD pin.
I think at this time they run the device in active mode, so I asked them to test the current and voltage at PVDD/DRAIN/nSLEEP/DVDD pin.
Then they cut the power line on DVDD and test the current on PVDD+DRAIN pin(they connect them together), it is still 16mA. It does not match to our datasheet. When nSLEEP = 0V, the device runs in sleep mode and Iq should be several uA.
Can you set PVDD/DVDD/nSLEEP to same voltage in EVM and test the current in PVDD? So that I can show them the result.
Did I miss anything to check?
Regards,
Peter