Other Parts Discussed in Thread: DRV10987
I am using the above evaluation module to drive a motor which has a rated power of 46W @ 24V supply. However, the torque the motor provide at max speed (or any speed) is not enough and does not seem to agree with motor specs. For example at the full speed, it draws only around 200mA average current with 24V supply. This is around 5W. The configuration used is as below (this is generated by the TI software). I like to know what kind of issue can cause this.
DRV10987 0x90 0xC1BA
DRV10987 0x91 0x4949
DRV10987 0x92 0x1
DRV10987 0x93 0x52
DRV10987 0x94 0x3BFF
DRV10987 0x95 0x3030
DRV10987 0x96 0x7A