Hi support team.
Is my understanding correct as following Figure?
If yes, the measured body diode VF value during the dead time period is 1.06V, and it is incomprehensible why it exceeds 1V.
Also, since this exceeds the absolute maximum ratings, is this considered a problem?
The measurement point is close to the device's output terminal AOUT1, so I don't think it depends on the layout.
The mainly parameters are below.
<Motor parameter>
Rs = 25ohm
Ls = 42mH
Best regards,
Higa