Other Parts Discussed in Thread: MCF8315A, MCF8315C
Hi Team,
Could you help share which EVM evaluation board for the DRV109XX can be used to drive a brushless DC motor for a mechanical hard drive? Thanks.
Best Regards,
Cherry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Could you help share which EVM evaluation board for the DRV109XX can be used to drive a brushless DC motor for a mechanical hard drive? Thanks.
Best Regards,
Cherry
Hi Cherry,
Can you help to clarify with some more details. You are already referring to EVM part number in the subject line. Do you have any specific electrical parameter and specification of the mechanical hard drive system ?
Thanks and Best Regards,
Venkatadri S
Hi Venkatadri S,
Thank you for the support.
Can you help to clarify with some more details. You are already referring to EVM part number in the subject line.
The EVM part number in the subject line is just to be filled in for raising the issue. No specific part has been selected yet.
Do you have any specific electrical parameter and specification of the mechanical hard drive system ?
For the electrical parameters of the mechanical hard drive motor, the drive voltage for the 3.5 inch disk is 12 V, the drive voltage for the 2.5 inch disk is 5 V and the drive voltage for the 2.5 inch disk is a sensorless brushless DC motor.
Using a typical brushless motor drive drives the hard drive motor, the speed can be adjusted by an analogue knob, but the exact speed cannot be set.
The customer is looking for a drive system that can precisely control the speed of the motor and can accommodate a 12-V drive voltage of 3.5-inch hard drives.
Thanks and regards,
Cherry
Hi Cherry,
I will reply by 22nd Friday for this. I want to provide couple of options and some more discussion needed.
Thanks and Best Regards,
Venkatadri S
Hi Cherry,
What is the power level of the drive? I am thinking to discuss about MCx port folio.
Thanks and Warm Regards,
Venkatadri S
Hi Venkatadri S,
What is the power level of the drive?
Around 10~15W.
Thanks and Regards,
Cherry
Hi Cherry,
Do you have any other constraint in terms of area, cost etc?
Can we check MCF8315A or MCF8315C RRY ?
Thanks and Best Regards,
Venkatadri S