Other Parts Discussed in Thread: DRV8424
hi experts
i want to use DRV8424 to control motor or Solenoids. from my narrow knowledge, if i want to control speed of motor accurately or control current of Solenoids accurately, i think we need to send high resolution PWM to device.
for example, in other words, device need to identify/respond the difference between 50% and 50.1%.
Q1: what accuracy range the input PWM signal can device identify?
Q2:what parameter/spec are list in datasheet to show the ability of identify input PWM signal accuracy?