This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8316AEVM: motor has no response

Part Number: MCF8316AEVM

Hi Team,

The motor do not respond when Run Mpet, could you help check why's this?

Thanks.

Best Regards,

Cherry

  • Hello Cherry,

    Does the nFAULT LED light up when attempting to run MPET? If the nFAULT LED is lit then I would recommend going though section 3.6 of the MCF8316A Tuning Guide. If the nFAULT LED was lit when the provided screenshot was taken then I would recommend going though section 3.6.1 specifically, since MPET_IPD is likely the fault that occurred.

    Regards,

    Joshua