Dears,
1. Can DRV10983Q1 set the PWM working range? Currently, we only see the minimum duty cycle setting. If it is less than 5%, it will output 5%, and if it is less than 1.5%, it will output 0; Is there a maximum duty cycle setting that outputs at the highest speed above 98% duty cycle?
2. Can PWM be set to correspond to the actual speed, such as my 30% duty cycle corresponding to 1000rpm?
4. What is the normal starting time for the motor? I have set the 1st and 2nd acceleration to the maximum and can reach the target speed within 8 seconds.
Many tks!