Part Number: DRV10964
Hello TI support Team,
i have an PCB-BLDC motor, 6coils und a flat disk with 8 magnets. To drive this motor i chose an DRV10964.
With 2 coils in series it has Phase to Phase resitor about 20Ohm, an inductance about 48uH and a Kt about 2,4 (125kHz / Vss = 600mV). Vcc ist 5V
I test different config settings und let the duty cycle increase.
It always turns out the same.
The disk aligns, it is accelerated nicely and the motor spin out until stop.
In the scope i can see the individual phases very clearly.
Align, open loop acceleration, HI-Z, closed loop, spin out.
I`m wondering why the driver stops and what lock kicks in to stop the motor.
Can you help me figure this out so I can improve the design?
Thank you.