1.Part number:MCF8315A.
Currently looking down the chip manual for the MCF8315A chip, I ran into some detail problems and need help to support them, thanks.
1. chip input voltage Pin pin is? Chip voltage supply range? The chip manual does not write.
2. Alarm Pin and nFault Pin specific pull high pull low output content difference is?
3. Is PWR an input or an output? The chip manual has PWR I, PWR O and PWR I/O, but there is also a PWR.
4. Can you explain the details of SOX Pin in detail?
5. How does the DACOUT2/SOX Pin convert SOX and DACOUT2 output methods?
6. SPEED Pin controls the difference between PWM and Frq inputs?
7. Under what conditions is I2C communication normally established, and is there a Pin pin control that causes it to be interrupted (Power Pin and Control Pin).
9. I2C write each byte need to delay 100 microseconds, that send a data need to delay how much time? Or no delay?
10. Currently our hardware is the same way I2C control two MCF8315A chip, how to send data to change the targetID of a separate chip, so that the two chips are controlled separately?